DNP3

Configure a NULL Pulse Action

A Pulse (NULL) has one action. Use the fields within the Actions section of the Pulse Action tab (or the <Pulse Type> tab on some drivers) to define the properties of the NULL action.

The Severity, Description, and Confirm fields are common to pulse actions on many drivers—for information, see Define the Actions that a Pulse Undertakes in the Geo SCADA Expert Guide to Core Point Configuration. Fields that are specific to DNP3 Pulse (NULL) Actions are explained below.


Disclaimer

Geo SCADA Expert 2022