DNP3

Download File

Associated with: DNP3 master outstations

Security permission required to access this pick action: Retrieve Data

Use the Download File pick action to download a file (for example, an ISaGRAF curve, or a log file) from the Geo SCADA Expert server to a DNP3 outstation.

Select the Download File pick action to display the Download File window. The content of the window varies, depending on the File Transfer Variation supported by the outstation (see Specify Which File Transfer Routines an Outstation Supports).

Where an outstation supports the Revised g70 Variations of File Transfer routines, the Download File window includes these fields:

Where an outstation supports the Legacy g70v1 File Transfer variation, the Download File window includes a single Filename field. Use the field to enter the name of the file that you want to download to the outstation and then select the OK button for Geo SCADA Expert to perform the download.

The location of the file on the server is specified as part of the Geo SCADA Expert Server Configuration (see Define the DNP3 Master File Transfer Parameters). The file has to be in the specified folder (or a subfolder within that folder) on whichever Geo SCADA Expert server is currently the main server.

The DNP3 outstation may impose filename restrictions on the files that are to be downloaded to it. See the outstation documentation regarding such restrictions.

Example:

The folder from which files on the current main server are downloaded to DNP3 outstations is set to:

C:\ClearSCADADB

An operator selects the Download File pick action on a particular DNP3 outstation and specifies the filename:

myfile.txt

On execution of the pick action, Geo SCADA Expert downloads the file myfile.txt from the server location C:\ClearSCADADB, to the DNP3 outstation.


Disclaimer

Geo SCADA Expert 2022