DNP3

Execute Remote Method

Associated with: DNP3 master outstations

The Execute Remote Method pick action is only available when a DNP3 outstation is also a Geo SCADA Expert DNP3 Slave Outstation
(see Specify Whether the Outstation is a Geo SCADA Expert DNP3 Slave Outstation).

Security permission required to access this pick action: Control

Use the Execute Remote Method pick action to execute a method (pick action) on a remote Geo SCADA Expert server. For example, to send a One Shot control to an outstation that is on another Geo SCADA Expert system.

Select the pick action to display the Execute Remote Method window. Use the fields in the window to specify the method that you want Geo SCADA Expert to perform on a remote item, and any parameters for that method:

If an Execute Remote Method action is used on your system on a regular basis, you might want to consider associating the Execute Remote Method with a Schedule. This would enable the method to be triggered automatically at regular intervals, and would avoid the need to manually specify the Object, Method and Parameter properties whenever it is triggered. For information on configuring a Schedule and using it to trigger a method on a regular basis, see Using Schedules to Automate Regular Functions in the Geo SCADA Expert Guide to Core Configuration.

For an Execute Remote Method action that is only used when required, you might want to consider:

Either of these options would avoid the need to manually specify the Object, Method and Parameter properties whenever the Execute Remote Method is triggered.


Disclaimer

Geo SCADA Expert 2022