DNP3

Specify the IIN Severity

Use these fields on the DNP3 tab to specify how Geo SCADA Expert processes any DNP3 IIN bits that are reported by the outstation. An outstation transmits DNP3 IIN bits if there is a problem at the outstation (see DNP3 IIN Flags).

IIN Severity

Use the first combo box to specify whether Geo SCADA Expert should process specific DNP3 IIN bits as an Alarm, Event, or None.

Use the second combo box to specify the severity of DNP3 IIN bits that are processed as Alarm or Event.

For further information on severities, see Defining Severities.


Disclaimer

Geo SCADA Expert 2022