DNP3

Specify the Status Points for which Data is Retrieved

Use the Points tab on the DNP3 Status Points Form to specify up to 10 Status Points for which Geo SCADA Expert is to retrieve data. For each Status Point, you need to configure the following:


Disclaimer

Geo SCADA Expert 2022