Configure DNP/IP Parameters

Use the fields in the DNP/IP Parameters section of the SCADAPack TCP/IP tab to specify the default DNP3 over IP properties for the SCADAPack E outstation.


Disclaimer

Geo SCADA Expert 2022