Configure Data Link Layer Properties

Use the three Data Link Layer properties, located in the Ports section of the Outstation Type tab, to specify how and when the SCADAPack E outstation will retry data link layer frames, and when the outstation will request confirmation of data link layer frames. These properties are only used by the outstation if the Function of the port is set to DNP3 or PPP/TCPIP and the port is used for sending DNP3 frames.

Data Link Retries and Data Link Confirm Timeout apply only if the Function of the port is set to DNP3 or PPP/TCPIP, and the Data Link Confirm Mode is set to an option other than Never.


Disclaimer

Geo SCADA Expert 2022