Configure Event Configuration

When a DNP3 device sends event data to a SCADA Master, each event is sent in a format known as a DNP3 Object. The DNP3 standard specifies Objects and Variations, which define the type and format of the data sent between DNP3 devices. For example, Object 2 is defined in the DNP3 standard as a binary event object and is used to send binary event data between DNP3 devices. Object 2, Variation 1 is defined as a binary event object with no time stamp, while Object 2, Variation 2 is defined as a binary event object with a time stamp. DNP3 Object/Variations are usually written in abbreviated notation. For example, Object 2 Variation 1 is written as g2v1

When a DNP3 event object with a time stamp is specified, the time stamp for the event is applied by the SCADAPack E outstation at the time the event occurs. When these events are received by Geo SCADA Expert, the Geo SCADA Expert server stores the values in its historic database, using the time stamp supplied in the event object. When a DNP3 event object with no time stamp is specified, the values are stored in the Geo SCADA Expert history database using the system time of the Geo SCADA Expert server at the time the events are received by the Geo SCADA Expert server.

In SCADAPack E versions before version 8.00, SCADAPack E outstations can generate events for physical inputs, and for derived points that have a static DNP3 object type. Specify the DNP3 input object/variation that applies to these points, using the DNP Object Type property on the relevant DNP3 SCADAPack Point Form (see Configure Common Properties of DNP3 SCADAPack Points).

Use the fields within the Event Configuration section of the outstation’s SCADAPack tab to specify the DNP3 event objects that the outstation uses to send event data to Geo SCADA Expert.

Each Events field is a drop-down list. Select one of the DNP3 event objects supported by the SCADAPack E outstation.

We recommend that you choose With Time events, so that Geo SCADA Expert logs the data using its original occurrence time, rather than the time that the event arrives at the server. Choose from:


Disclaimer

Geo SCADA Expert 2022