Configure the Firmware Image Properties

Use the fields within the Firmware section of the SCADAPack tab to define the properties associated with downloading operating system firmware to the outstation. In order to configure these Firmware properties successfully, a suitable DNP3 SCADAPack Firmware Image item has to exist in the Geo SCADA Expert database (see Configure a DNP3 SCADAPack Firmware Image Item).


Disclaimer

Geo SCADA Expert 2022