Display Historically Stored Profile Data

If a DNP3 SCADAPack point has a current value and/or limit(s) that are profile-controlled and that profile data is stored historically, you can display the historic profile data in either of two ways:

Further Information

Trends: see the Geo SCADA Expert Guide to Trends.

Producing Custom Lists: see Custom Lists in the Geo SCADA Expert Guide to Lists.

CDBProfileHistoric database table: see the database Schema.

Using the Database Schema: see Working with the Database Schema in the Geo SCADA Expert Guide to the Database.


Disclaimer

Geo SCADA Expert 2022