Downloaded Security Description

Associated with: DNP3 SCADAPack E Outstations and DNP3 SCADAPack Remote E Outstations that use DNP3 secure authentication.

This status attribute indicates the Description that was entered for the .rtk file when it was imported into the Geo SCADA Expert database (see Import Security Configuration).

The attribute is only displayed if the Download Security Configuration pick action has been used to successfully download a security configuration file to the outstation. The security configuration file comprises an .rtk file that has been imported into Geo SCADA Expert.

Use this status attribute in conjunction with the Downloaded Security File attribute to ascertain information about the .rtk file that was last downloaded to the outstation.


Disclaimer

Geo SCADA Expert 2022