File Restrictions

The files that you download to a SCADAPack E outstation have to comply with the following conventions. Where a file name needs adjusting to conform to these requirements, you can do this by renaming the file (see Specify the Properties of a File in a SCADAPack E Outstation’s Configuration), rather than renaming the original copy of the file.

If a file does not comply with these limitations or displays any invalid characters, the OK button on the Properties window will appear ‘grayed out’ and unavailable for use.


Disclaimer

Geo SCADA Expert 2022