Input Power Low

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve SCADAPack ES Remote I/O information.

This status attribute indicates whether the power being used to run the remote I/O module is low.

Possible states: True, or False.

Do not confuse this status attribute with the Internal Battery Low attribute.


Disclaimer

Geo SCADA Expert 2022