RemoveFile

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations.

Security permission required to access this method: Configure.

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

Use the RemoveFile method with care. Ensure that the file is no longer required or in use before attempting to remove the file from the database.

Failure to follow these instructions can result in unexpected loss of outstation functionality.

Use this method to remove a file from a DNP3 SCADAPack E outstation in the Geo SCADA Expert database.

This method is the equivalent of removing a file by using the Remove button on the Configuration Setup window (see Remove a File from a SCADAPack E Outstation’s Configuration).

Argument:


Disclaimer

Geo SCADA Expert 2022