Specify how the SCADAPack Outstation Handles any Pulse Action Events

The RTU Event property applies to DNP3 SCADAPack Pulse Actions that have a Point Type other than Physical Output, and a Point Data Class of Class 1 Event, Class 2 Event, or Class 3 Event (see Configure Common Properties of DNP3 SCADAPack Points).


Disclaimer

Geo SCADA Expert 2022