System Color Priorities

Each system color is assigned a level of importance, depending on the state that it represents. Geo SCADA Expert uses the hierarchy to ascertain the color that it assigns to each database item.

This section comprises charts that indicate which system foreground color takes priority when a DNP SCADAPack outstation or point is in a particular state:

If more than one state applies simultaneously, the higher-priority color takes precedence until that state no longer applies.

For more information on system color priorities, and for charts that indicate the priority of states represented by background colors, see System Color Priorities in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2022