Trend Inhibit Alarm

Associated with: DNP3 SCADAPack Analog, Binary, and Counter points.

This status attribute indicates whether Geo SCADA Expert’s last attempt to download the configuration that causes the outstation to start or stop sampling the point’s data was unsuccessful. Geo SCADA Expert attempts to download such configuration whenever the Enable All Trends or Disable All Trends pick action is triggered.

For example, the download would not succeed if communications were lost during the download, or an attempt was made to enable or disable DNP3 SCADAPack Trend sampling on a point for which such configuration did not yet exist in the outstation.

Possible states: Displays one of the Standard Alarm States.

Also see Trending Inhibited.


Disclaimer

Geo SCADA Expert 2022