UpdateFileProperties

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations

Security permission required to access this method: Configure

Use this method to update the property parameters for a file that exists in a DNP3 SCADAPack E outstation in the Geo SCADA Expert database.

This method is the equivalent of updating the file properties via the Properties button on the Configuration Setup window (see Specify the Properties of a File in a SCADAPack E Outstation’s Configuration).

Arguments:


Disclaimer

Geo SCADA Expert 2022