Methods

There are two types of method:

Each method has a unique name in its database table and may have arguments. The arguments (also referred to as parameters) are used to pass information to the system when the method is executed. For example, the Control method on an output point has an argument to specify the value to which the point is set.

For calculation methods, the last argument is the value that is returned by the method. When you use the Database Schema to view a calculation method, the last argument of the calculation method has a [retval] prefix.

You can use the Geo SCADA Expert Database Schema to access information about the methods that are associated with each class (see Class Information).


Disclaimer

Geo SCADA Expert 2022