Cancel Control

Associated with: Output points and pulse actions on simple drivers

Security permission required to access this pick action: Control

This pick action is only available on a point or pulse action when a Control request is presently active, or is awaiting execution.

Use the Cancel Control pick action to cancel the currently active control.

Also see Abort Pulse.

If using this pick action with the Automation Interface, you need to specify the method name ControlCancel.


Disclaimer

Geo SCADA Expert 2022