Channels

The Geo SCADA Expert server runs drivers, many of which communicate with outstations and similar devices via Channels. Depending on the system setup, a channel will use one of these types of communication:

Each channel is represented in the Geo SCADA Expert database by a Channel database item. You need to add and configure the type of channel that corresponds to the type of protocol and communications being used by your system. You can perform actions on channels via pick action menus (also referred to as context sensitive menus).


Further Information

For information on configuring specific types of channel, see the relevant driver guide.

For general information on configuring channels, see the following:

Actions Associated with Channels on Simple Drivers.

Actions Associated with Channels on Advanced Drivers.


Disclaimer

Geo SCADA Expert 2022