Enable Set
            Associated with: Outstation sets
Security permission required to access this pick action: Disable Points
Use this pick action to place an outstation set In Service. Triggering the action changes the outstation set's configuration so that its In Service property is enabled. Providing that any items on which the outstation set is dependant are also In Service and have valid configuration, the outstation set will become active. (With an outstation set other than a PSTN outstation set, dependants include the channel(s) with which the outstations in the set communicate.)
The Enable Set pick action is only available for an outstation set:
- That is not In Service
 - For which your User Account is allocated the Disable Points security permission.
 
Also see Disable Set.
If using this pick action with the Automation Interface, you need to specify the method name Enable.