Fallback

Associated with: Direct or Shared outstations that can fallback to PSTN.

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Use the Fallback pick action with care. Always check an outstation’s current activity before deciding whether to use this action.

To check whether an outstation is currently processing a request, look at its entry in the Outstations List’s Current Request column. You can also check an outstation’s current activity via, for example, the Events List or the outstation’s Status display.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

With an outstation on which PSTN fallback is available, communications will automatically ‘fall back’ to using an available PSTN channel, should Geo SCADA Expert detect that the direct communications has failed (see Direct - PSTN Fallback). Similarly, if an outstation is configured to accept Download Configuration via PSTN, communications will automatically switch to PSTN for the duration of a download (see Define an Outstation’s PSTN Properties).

In addition, you can use the Fallback pick action to change the type of communications being used for the outstation at any time (for instance, if maintenance work needs performing on the direct channel(s)).

The Fallback pick action is only available on an outstation on which:

Select the Fallback pick action to display the Fallback window. Select the required option from the Action combo box. Depending on the type of communications that Geo SCADA Expert is currently using to communicate with the outstation, one of these options will be available for selection:


Disclaimer

Geo SCADA Expert 2022