Last Incoming Call Lost Comms
Associated with: PSTN outstations or outstations on which PSTN fallback is enabled
This attribute displays the date and time of the last incoming call for which communications were established, but which then terminated unexpectedly. The attribute is only displayed once such a call has occurred.
Example:
20/Mar/2008 12:41:08.140
Also see the Incoming Calls attribute, which provides a summary of the incoming calls since the statistics were last reset.