Reset Outstation
Associated with: Outstations on drivers that support this feature
Security permission required to access this pick action: Diagnostics
LOSS OF COMMUNICATION
Use the Reset Outstation pick action to reset an outstation. The type of reset that is performed depends on the protocol—refer to the outstation’s product documentation for information. With outstations that support more than one type of reset, a window is displayed, offering a set of reset options. The driver-specific documentation explains any such options where they exist.
If using this pick action with the Automation Interface, you need to specify the method name Reset.