Configuring an EcoStruxure Web Services Server

For every server with which you want Geo SCADA Expert to communicate using the EcoStruxure Web Services protocol, you need to configure an EcoStruxure Web Services Server in the Geo SCADA Expert database.

Before configuring an EcoStruxure Web Services Server in the database, carry out any necessaryPreparation. Then use the fields on the EcoStruxure Web Services Server Form to configure the EcoStruxure Web Services Server database item(s) on your system.

The Form has several tabs. Use the fields on the Server tab to define the connection properties that are required for successful communications with the node on which the EWS data is located (see Configure the EcoStruxure Web Services Server Properties)(see Configure the EcoStruxure Web Services Server Properties)

For information on the fields on other tabs, see Tabs That are Common to Many Configuration Forms in the Geo SCADA Expert Guide to Simple Drivers.

For information on the minimal amount of configuration that you can undertake to produce a functional EWS Server in Geo SCADA Expert, see Minimum Configuration.


Disclaimer

Geo SCADA Expert 2022