Create an EtherNet/IP Direct Channel

When you create the channel, you can leave most of the fields at their default values. The only fields that you need to change for this tutorial are:

Save the configuration.

For further information on configuring an EtherNet/IP Direct Channel, see Configure an EtherNet/IP Channel.

Once you have configured the channel, you can proceed to Create an EtherNet/IP Direct Outstation Set.


Disclaimer

Geo SCADA Expert 2022