Create an EtherNet/IP Direct Outstation

In Geo SCADA Expert, you use an Outstation database item to represent an Allen-Bradley controller.

When you create the outstation, you can leave most of the fields at their default values. The only fields that you need to change for this tutorial are:

Save the configuration.

For further information on configuring an Outstation, see Configure an EtherNet/IP Outstation.

Once you have configured the outstation in Geo SCADA Expert, you can proceed to Create an EtherNet/IP Analog Point.


Disclaimer

Geo SCADA Expert 2022