COSH
The COSH function is a mathematical function that returns the Hyperbolic Cosine of a number. The COSH function returns a real value.
Function Name |
COSH |
Description |
Returns the Hyperbolic Cosine of a number. |
Arguments |
COSH(INTEGER OR REAL) The value can be an integer or a real floating value—see Number (Integer or Real). |
Returns |
The Hyperbolic Cosine of a number. This is of the same type as the input (INTEGER or REAL). |
Example:
COSH(PI())
The output is 11.59.