LEFT
The LEFT function returns a specified number of characters from the left side of a string.
Function Name |
LEFT |
Description |
Returns a specified number of characters starting from the left of an input string. |
Arguments |
LEFT('STRING', LENGTH) Where:
|
Returns |
STRING. The returned value is a string value that consists of the specified number of characters. The characters are taken from the defined input string, beginning at the first character from the left of the string. |
Example:
The expression:
LEFT( 'Pipeline', 4 )
returns:
Pipe
(4 characters starting from the left of the 'Pipeline' string).