LOG
The LOG function is a mathematical function that returns the natural logarithm of a number as a real value.
Function Name |
LOG |
Description |
Returns the natural logarithm of an input number as a real value. |
Arguments |
LOG(INTEGER or REAL) The input number has to be greater than 0. For more information, see Number (Integer or Real). |
Returns |
REAL The natural logarithm value of the input number. |
Example:
LOG(2)
The output is 0.69