TAN

The TAN function is a mathematical function that returns the Tangent (radians) of a number. The TAN function returns a real value.

Function Name

TAN

Description

Returns the Tangent (radians) of a number.

Arguments

TAN(INTEGER or REAL)

Where:

  • INTEGER or REAL is a numerical expression that defines the value on which the TAN function is applied.

For more information on integers and real values, see Number (Integer or Real).

Returns

REAL

The Tangent (radians) of a number.

Example:

TAN(1.2)

The output is 2.57


Disclaimer

Geo SCADA Expert 2022