DeviceConfiguration Group

The FloBossDemo.sde file includes a DeviceConfiguration group.

This group contains points that are configured to show different types of information about a FloBoss. The intent of this group is to demonstrate how to use the Geo SCADA Expert FloBoss Driver to read configuration information from a FloBoss.

Some points, like ContractHour, have the Control aggregate enabled. You can right-click on this point in the Database Bar, select the Control option, and enter a new contract hour for the FloBoss device.

The points in this group are displayed and manipulated from the Configuration Mimic in the Mimics Group. Each of the points in this group are attached to the ScannerConfig scanner.


Disclaimer

Geo SCADA Expert 2022