How can I read the gas composition for a specific run?

The FloBossDemo.sde file includes demonstrations of how to read the gas composition for a run.

In summary, you will need to set up a FloBoss Numeric Point for each parameter that you want to read and then configure that point with the appropriate TLP. For example, the Type and Parameter for nitrogen is 46 and 23. The run number will determine the Location value.


Disclaimer

Geo SCADA Expert 2022