Automation Interface Methods
In addition to the pick actions that are available in ViewX, additional methods (pick actions) are available using the Geo SCADA Expert Automation Interface.
The topics in this section provide information about methods that are specific to the AVEVA Historic Data Export driver.
The following method is available on AVEVA Historic Data Export items when using the Automation Interface:
To find out about the methods that are available for each type of database item, please refer to the Database Schema (see Working with the Database Schema). The Database Schema provides details on the name and arguments of each method, so that you can call the methods from your own programs and scripts.
Be aware that there might be references to 'Wonderware Historian' in the Database Schema. 'Wonderware Historian' is the name by which the AVEVA Historic Data Export driver was previously known.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.