ServerTimestamp

Description

This property determines whether the timestamp of the data value at the time of acquisition is overwritten with the local timestamp of the historian server when the data value is received by that historian server. The property value indicates whether the historian uses server timestamping for the tag. If the property value is True, then the historian uses server timestamping.

Note that if a fast-changing tag is configured to use server timestamping, the packet of data that is sent to the storage subsystem may contain multiple data values with the same timestamp. This may affect data calculations, such as for swinging-door storage. This property applies to all tag types.

Geo SCADA Expert Metadata Field

WH_ServerTimestamp

Default Value

The default value for this property is False.

Type

Boolean.


Disclaimer

Geo SCADA Expert 2022