StorageRate
Description
The rate at which the historian stores the tag value if the storage type is Cyclic. This property applies only to analog tags. In Geo SCADA Expert the TagStorageType is always set to Forced, and therefore this property is not applicable.
Geo SCADA Expert Metadata Field
WH_StorageRate
Default Value
The default value for this property is 0.
Type
Unsigned Long.