Supported Versions of AVEVA Applications with Historians

You use this driver to export Geo SCADA Expert historic data to a historian in an AVEVA application such as AVEVA Historian (formerly Wonderware Historian) or AVEVA Insight (formerly Wonderware Online).

The earliest version of AVEVA Historian with which the driver is compatible is Wonderware Historian (AVEVA Historian) 2014 R2 SP1 Patch 02.

Except where stated otherwise for specific features, this driver supports functionality that is available in AVEVA Historian up to and including the following version:

Wonderware Historian (AVEVA Historian) 2017 Update 3

The AVEVA Historic Data Export driver provided with Geo SCADA Expert is designed to be forward compatible, so should also be able to interface with later versions of historians in supported AVEVA applications.

The RenameTag method is supported by AVEVA Historian (formerly Wonderware Historian) only, from the following version onwards: Wonderware Historian (AVEVA Historian) 2017 Update 2 with hotfix CR L00149314. (It is not supported by AVEVA Insight (formerly Wonderware Online).)

Further Information

Upgrade Guidelines.


Disclaimer

Geo SCADA Expert 2022