Reset Poll Statistics
Associated with: ICMP Digital Points
Security permission required to access this pick action: Diagnostics
Use the Reset Poll Statistics pick action to reset the Poll Times statistics for a point. The statistics indicate, for example, the number of times that the ICMP driver has polled the device with which the point is associated (see Poll Times).
If using this pick action with the Automation Interface, you need to specify the method name ResetStatistics.