Configure the Counter Interrogation Intervals

The IEC 60870-5 driver supports regular interrogation of outstations for counter data. Some outstations are set to report their counter data to the SCADA master (Geo SCADA Expert) automatically. Other outstations might only report their counter data on interrogation by the SCADA master. Similarly, an outstation might ‘freeze’ and/or reset its counter values automatically, or only on request (see Counter Operation Modes and Interrogation Requests).

Geo SCADA Expert can send requests to an outstation to trigger it to perform operation(s) on its counters, or, if supported by the outstation, to perform operation(s) on only those counters that are associated with a particular counter interrogation group. An outstation might support up to four counter interrogation groups.

Refer to an outstation’s interoperability Profile document for information on:

You also need to be aware of:

In ViewX, you can specify whether Geo SCADA Expert is to send periodic requests that will trigger the outstation to perform certain operations on its counters. To do this, you need to use the fields in the Counter Interrogation Intervals section on the EIC 60870-5 tab of the IEC 60870-5 Outstation Form. For instance, if the outstation does not report its frozen counter values automatically, you can set it to report the values at regular intervals. This is achieved by selecting the Request check box and defining a suitable Interval and Offset.

For information on which of the Request, Freeze, and Reset check boxes to select, see Counter Operation Modes and Interrogation Requests.

In each instance, use the Interval field to specify how often Geo SCADA Expert sends the selected counter request(s) to the outstation. Use the Offset field to specify the synchronization offset—the amount of time that occurs from midnight before Geo SCADA Expert sends the first request to the outstation for each counter interrogation group. Specify both the Interval and the Offset in the OPC Time Format.

In addition to the above, you can specify whether Geo SCADA Expert is to interrogate an outstation for counter data as soon as it establishes communications with that outstation (see Specify the Operations Performed on Communications Establishment).

If an outstation supports counter data, map that data to IEC 60870-5 Analog Point(s) in the Geo SCADA Expert database, in order to use that data within Geo SCADA Expert (see Configuring Analog Points).


Disclaimer

Geo SCADA Expert 2022