Get Directory

Associated with: IEC 60870-5 Outstations

Security permission required to access this pick action: Retrieve Data

Use the Get Directory pick action to obtain a list of binary files on an IEC 60870-5 outstation. This is useful when you need to ascertain the locations and names of files on an outstation—for instance, before uploading files from, or downloading files to that outstation.

Select the Get Directory pick action to display the Get Directory window. The window has these fields:

If using this pick action with the Automation Interface, you need to specify the method name Directory.

Example:

This directory listing for IOA 0 shows that ten files exist at that address in that particular outstation.


Disclaimer

Geo SCADA Expert 2022