Specify the Format in which to Transfer Control Data

This section applies to IEC 60870-5 Analog Output Points only.

The IEC 60870-5-101 protocol defines a number of ASDU formats (ID 48 to ID 51) that can be used by Geo SCADA Expert for sending analog control information to the outstation.

The IEC 60870-5-104 protocol defines the above ASDU formats along with an additional set of ASDU formats (ID 61 to ID 64). The latter formats allow Geo SCADA Expert to include the time with each control message that it sends to the outstation. The IEC 60870-5-104 protocol includes these additional formats as the nature of TCP/IP means that control packets may arrive at the outstation a significant amount of time after they were sent. By using one of these formats, the outstation is able to reject any control requests that are deemed too far in the past. (The exact functionality is dependent on the manufacturer’s implementation.)

Each analog output on an outstation supports one or more of the ASDU formats mentioned above (refer to the outstation’s interoperability Profile document for information on which formats are supported). When Geo SCADA Expert transmits a control request for an IEC 60870-5 analog output point, it uses the format that is specified in the point’s configuration. For this reason, you need to configure the IEC 60870-5 analog output points in the database to use the same formats as the points they represent on the outstation. To do this, use the IEC 60870-5 Type field on the Control tab of the IEC 60870-5 Analog Output Point Form.

Use the field’s combo box to select the required control format:


Disclaimer

Geo SCADA Expert 2022