Typical Identification Values for KEMA points
The following table lists the defined data types for KEMA points and the corresponding Type Identification Values.
| Type of Measurement | Type Ident. Value | Data type description |
|---|---|---|
| Analogue values | 9 | Measured value: normalized value |
| 10 | As above with time tag | |
| 11 | Measured value: scaled value | |
| 12 | As above with time tag | |
| Digital command | 45 | Single command |
| Analog command | 48 | Setpoint command: normalized value |
| 49 | Setpoint command: scaled value | |
| Digital status | 1 | Single point information |
| 2 | As above with time tag | |
| Counter values | 15 | Integrated total |
| 16 | As above with time tag |