Configure the COMTRADE Files Polling

COMTRADE files contain the waveform data. The IEC 61850 driver supports retrieval of COMTRADE files as defined by the IEC 61850 standard, periodically transferring them to a local directory. These files are stored in an IED in pre-determined folders. The driver periodically checks the available files in the IED root directory to determine if there are any new files. If the driver finds new files, it will download and save them locally on the Geo SCADA Expert machine.

To configure the COMTRADE files polling section, complete the following fields:

When the driver requests the files information, the device must send the flat list of file paths in the device root and subdirectories. The file transfer will not work if the device only sends the list of files in the specified directory.


Disclaimer

Geo SCADA Expert 2022