Configure the Write Properties of an IEC 61850 Digital Point
IEC 61850 Digital Points that are created for the corresponding IEC 61850 Data Attributes will have a Write tab on the Digital Point Form. To create IEC 61850 Digital points you should use an SCL file which defines the relevant Data Attributes. You cannot create IEC 61850 Digital points with a Functional Constraint of CO. The Write tab does not have the Control Options section, as they cannot be created to represent an IEC 61850 data object where these options are used.
Use the Write tab to:
- Define the Control Settings for a Digital Output Point
- Promote Retrieval of Data Associated with Controls (see Promoting Scanning of Outstations Associated with Controls).
- Update an Output Point's Value Immediately Following a Successful Control Action.