Control Operation Parameters

Control parameters that are set automatically are:

Control parameters that can be set manually in the control object are:

Other important parameters are listed below:

Depending on the control model of the data object, there may also be a few additional parameters:


Disclaimer

Geo SCADA Expert 2022