General Properties

Use the fields at the top of the <Point Type> tab of the appropriate Point Form to define the general IEC 61850 settings for a point. Depending on the type of the Point, some or all of these fields may be available. These fields are common to many IEC 61850 points:


Disclaimer

Geo SCADA Expert 2022