Logical Device
You use a Logical Device database item to represent a part of the address space of the IED from a substation with which Geo SCADA Expert is to interact using the IEC 61850 protocol. You require one Logical Device database item per part of the IED address with which Geo SCADA Expert is to interact.