Common Point Properties

Use the fields at the top of the Analog Point tab to Configure Common Point Properties. Fields that are specific to analog points are explained below.

Channel Number

Only applies to Hardware I/O types. Use the Channel Number field to specify the channel number for the point, in the range 1 to 8.


Disclaimer

Geo SCADA Expert 2022