Scan Statistics

Associated with: Kingfisher Direct channels

This status attribute indicates the time period for which the Scan Duration, Scan Count and Message Count statistics apply.

If the Reset Statistics pick action has been used to reset the statistics, two Scan Statistics entries are displayed. The first entry indicates the date and time from which the current set of statistics commenced; the second entry indicates the time period to which the previous set of statistics applies.

Example:

Since Jul/12/2010 15:56:51.830

If the statistics have been reset, a second entry will display this type of information:

Between Sep/29/2009 14:37:43.473 and Jul/12/2010 15:56:51.830


Disclaimer

Geo SCADA Expert 2022